CE marking

The control cabinet and machine have different numbers on the CE mark. Is this permitted?

Control cabinets are often certified in accordance with the Low Voltage / EMC Directive, particularly if the control cabinet comes from another manufacturer. So it is both possible and permitted for the machine and control cabinet to have difference CE marks.
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
Was this article helpful?