CE marking

What information/standard must be stated in the declaration of conformity: EN ISO 13849-1:2008 or EN ISO 13849-1:2008/AC:2009?

There is no generally applicable specification for naming the applied standard.

From practical experience, we recommend the following information:
EN ISO 13849-1:2008 Safety of machinery - Safety-related parts of control systems - Part 1: General principles for design (with amendment AC:2009)