CE marking

We would like to relocate within the EU a machine that has been built and certified in accordance with the Machinery Directive 98/37/EC. May this machine be put back into service in this way?

If the machine is to be put back into service in the same state, then no measures are required with regard to the Machinery Directive 2006/42/EC. In this case the CE mark can be regarded as a type of passport within the EU.