Is there a standard that states how high the reduced speed may be, on conveyors for example, if the conveyor is not enclosed?

Safe reduced speed and continuous flow conveyors

The C standard EN 619:2002 for continuous handling equipment and systems only states speed for cases in which people may travel on the conveyor. These are:

Continuous flow conveyors on which persons may travel:

  • Floor level: Conveying speed of 0.3 m/s
  • 0.3 m above floor level: Conveying speed of 0.15 m/s
  • Full railings: Conveying speed of 0.5 m/s

VDI 2854 also deals with the issue of safe, reduced speed. This states that a speed is deemed to be safe if the person has time to escape from a hazardous event.

 

Head office

Pilz Australia Safe Automation
Unit 1, 12-14 Miles Street
Mulgrave, Melbourne, Victoria 3170
Australia

Telephone: +61 3 9560 0621 / 1300 723 334
E-Mail: safety@pilz.com.au

Technical Support

Telephone: +61 3 9560 0621
E-Mail: techsupport@pilz.com.au

Was this article helpful?