The safety assessment is carried out independently from ROS: In our system, safety is guaranteed by incorporating a safety controller. This monitors the safety-related aspects and can stop the robot safely if needed (STO).
ROS is “notified” immediately about the current status and other safety-related details via a direct communication channel between ROS and the safety controller.
Robotics
How are safety requirements implemented with ROS?
Head office
Pilz Australia Safe Automation
Unit 1, 12-14 Miles Street
Mulgrave, Melbourne, Victoria 3170
Australia
Telephone: +61 3 9560 0621 / 1300 723 334
E-Mail: safety@pilz.com.au
Technical Support
Telephone: +61 3 9560 0621
E-Mail: techsupport@pilz.com.au
Was this article helpful?