The contacts can be used for cascading between two PNOZmulti systems or to exchange a safe signal. The contact CO+ can be used as a standard output.
Small controllers
Configurable safety systems PNOZmulti
What is the function of the contacts CI+/CI- and CO+/CO- on the base units PNOZmulti (PNOZ m1p, PNOZ m2p, PNOZ m3p, serial and ETH)?
Head office
Pilz Australia Safe Automation
Unit 1, 12-14 Miles Street
Mulgrave, Melbourne, Victoria 3170
Australia
Telephone: +61 3 9560 0621 / 1300 723 334
E-Mail: safety@pilz.com.au
Technical Support
Telephone: +61 3 9560 0621
E-Mail: techsupport@pilz.com.au
Was this article helpful?