Small controllers

Configurable safety systems PNOZmulti

How can I use the extended virtual I/Os via fieldbus?

Firstly, the I/O size of the fieldbus module must be set from 24 to 128 in the hardware configuration. Next, Table 9 – Segment 1 of the Multi can be requested from the higher level controller. The communication manual describes the necessary steps in detail.