- The PNOZmulti cycle time is 10-15 ms. This time depends on the project size.
- The current cycle time of the PNOZmulti can be displayed in the "Status" window as soon as dynamic program display is started. The status LED can also be found there.
- On the PNOZmulti mini and PNOZmulti 2, the current cycle time can be shown on the display.
Small controllers
Configurable small controllers PNOZmulti
What is the reaction time of the small controllers PNOZmulti?
Head office
Pilz Australia Safe Automation
Unit 1, 12-14 Miles Street
Mulgrave, Melbourne, Victoria 3170
Australia
Telephone: +61 3 9560 0621 / 1300 723 334
E-Mail: safety@pilz.com.au
Technical Support
Telephone: +61 3 9560 0621
E-Mail: techsupport@pilz.com.au
Was this article helpful?