Small controllers

Configurable small controllers PNOZmulti

With some small controllers PNOZmulti there is a "coated version" / types with an additional -T in the name. What does this mean?

On the "Coated version" / -T-type, the circuit board is covered with a protective coating. Benefit: the PNOZmulti is better protected against environmental influences. (Dust, swarf, corrosive gases etc.). The possibility of short-term condensation and an extended temperature range are other benefits.
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
Was this article helpful?