In connection with the safety relay PNOZ, what is the meaning of an automatic, manual and monitored start?

Safety relays PNOZ X

  • Automatic start: The relays energise as soon as the input circuit is closed.
  • Manual start: A rising edge is expected in the start circuit.
  • Monitored start: A falling edge is expected in the start circuit.

 

Head office

Pilz Australia Safe Automation
Unit 1, 12-14 Miles Street
Mulgrave, Melbourne, Victoria 3170
Australia

Telephone: +61 3 9560 0621 / 1300 723 334
E-Mail: safety@pilz.com.au

Technical Support

Telephone: +61 3 9560 0621
E-Mail: techsupport@pilz.com.au

Was this article helpful?