Yes, provided the PMI-PRO project has at least version 5.50 SP7 and contains drivers that also use Zenon. The editor must be launched in 32-bit mode.
Operating and monitoring
Operator terminals PMI
Can an older PMI-PRO project be converted into a Zenon version from 7.00?
Head office
Pilz Australia Safe Automation
Unit 1, 12-14 Miles Street
Mulgrave, Melbourne, Victoria 3170
Australia
Telephone: +61 3 9560 0621 / 1300 723 334
E-Mail: safety@pilz.com.au
Technical Support
Telephone: +61 3 9560 0621
E-Mail: techsupport@pilz.com.au
Was this article helpful?