Australia | english

Small controllers

Configurable small controllers PNOZmulti

What is the reaction time of the small controllers PNOZmulti?

  • The PNOZmulti cycle time is 10-15 ms. This time depends on the project size.
  • The current cycle time of the PNOZmulti can be displayed in the "Status" window as soon as dynamic program display is started. The status LED can also be found there.
  • On the PNOZmulti mini and PNOZmulti 2, the current cycle time can be shown on the display.