Australia | english

Controllers

Software

What is the IP address of the PSS ETH2 during initial commissioning?

DHCP functionality is activated on the ETH2 interface during initial commissioning. If the network contains a DHCP Server, the IP address is assigned to the ETH2 via the DHCP Server.

If the network does not contain a DHCP Server, the ETH2 interface assigns a default IP address from the range 169.254.60.1 - 169.254.60.14.