Australia | english


PLC controllers and I/O systems

How can the control head be reset to the factory default settings?

Original reset: carry out the following steps <10 s

  • Switch off voltage to PSS
  • Remove SD card
  • Switch on voltage to PSS
  • Press reset button >5s until DIAG-LED flashes
  • Release reset button
  • Press reset button
  • Release reset button

The control head will now have the following default settings:

  • Device name: PSS__
  • IP address: to (Auto-IP mechanism)
  • Subnet mask:
    SD card can be formatted via a PC.