With its innovative products, Pilz has written industrial history. In the field of control technology we were one of the first suppliers worldwide. In 1986 Pilz developed a compact circuit within a housing, which replaced the laborious process of wiring contactors. Pilz’s development engineers built on this existing expertise to design the PNOZ trademark. The E-STOP relay PNOZ was the first safety relay and to date is the most widely used worldwide. As the epitome of safety relays, a world without it is no longer conceivable.
Technological milestones


The origin of today's programmable safety controllers goes right back to 1969, when Pilz developed the EUROPILZ SYSTEM. The system comprises a complete range of plug-in Eurocards, used to build industrial controllers. On this basis Pilz was able to respond to the market's requirement for "free programming“ with the PC4K controller in 1974. This was followed by the PITRONIK compact controller in 1976, plus the PITRONIK P8, which was freely programmable using a programming set and standard PCs. The first programmable safety controller PSS 3000 appeared in 1995. With this system Pilz broke new ground, moving from electromechanics towards an electronic solution for safety-related applications.
At a glance: important innovations from Pilz
1964 | One of the first relays – mercury timer relay |
1968 | First two-hand control relay - S-68 series |
1969 | First control system – EUROPILZ SYSTEM |
1974 | First programmable controller – PC4K |
1986 | High-performance PLC – PITRONIK P9 |
1987 | E-STOP relay PNOZ |
1995 | First programmable safety controller PSS 3000 |
1999 | First safe fieldbus system – SafetyBUS p |
2002 | First configurable small controllers – PNOZmulti |
2004 | First coded safety switch PSENcode |
2006 | First safe camera system – SafetyEYE |
2009 | First automation system for safety and automation – PSS 4000 |
2013 | First internationally certified qualification for machinery safety – CMSE® |
2016 | Web-based visualisation software – PASvisu |
2016 | First type 3 light curtain - PSENopt II |
2018 | First service robotics modules - PRBT, PRCM, PRTM, ROS |
2018 | First security product - SecurityBridge |
2019 | CECE - First certified qualification for CE marking |
Top developments: from a mercury relay to a complete robot solution
First industrial electronics equipment manufacturer
Together as a team Pilz initiated important standards and directives, to achieve a uniform view of plant safety. That’s as true today as it was then. Even back in the 70s, Pilz was setting benchmarks in the standardisation of electronic components. Together with major industries, Pilz developed a standard with the series mounting dimension of 35 mm, which was ultimately accepted as the standard.
As a result, the automation company became the first industrial electronic equipment manufacturer to market DIN electronic relays. The standard timer relay from the “N-35” series could be clipped directly on to a standard rail, enabling much faster installation for customers. Later the relays were joined by further products on this basis, such as monitoring or two-hand control relays, and so could be used for additional applications.

Together to success: Pilz's companions along the way
This is where history comes alive: Listen to our former employees to discover more about the time when important technological milestones were developed and how they witnessed this special family and company history.
Pilz Australia Safe Automation
Unit 1, 12-14 Miles Street
Mulgrave, Melbourne, Victoria 3170
Australia
Telephone: +61 3 9560 0621
E-Mail: safety@pilz.com.au