Australia | english

Ostfildern, 11 Nov. 2014

New web-based visualisation software PASvisu by Pilz - Your automation at a glance

With the web-based visualisation software PASvisu Pilz is launching a high-performance yet simple to use software package for operating and monitoring. The company has developed a platform-independent visualisation package based on the latest web technologies such as HTML 5, CSS3 and JavaScript PASvisu is operated intuitively and provides design freedom for projects: it gives users of Pilz control solutions a complete view of their plant. With PASvisu, Pilz is underlining its claim as a complete safe automation supplier.

The visualisation software enables visualisation projects to be created and configured simply using the PASvisu Builder.
Access to all the data in an automation project, including all process variables and OPC namespaces, means there is no need to enter and assign variables manually, a process that is prone to errors. Information such as the project's check sum or the firmware version of the controller head module can also be called up, for example.

Individual visualisation via tiles
Selectable styles via CSS3 provide a uniform, consistent image across the project at the click of a mouse.
Pre-defined graphic input and display elements, called tiles, already provide all the relevant properties, such as prefix, suffix and error status. There is no need to create and group individual elements manually. The tile is positioned on the configuration page simply via drag and drop and is then filled with the relevant data. Even as the variable name is typed in, the variable is automatically filtered out and simultaneously linked to the tile. That way projects can be handled quickly and without error.

Graphical block diagnostics and simulation
Other miscellaneous information needed in the visualisation project is also processed automatically. Also, changes in the automation project are synchronised automatically and displayed in the PASvisu Builder. Thanks to automatic synchronisation, users are always working with the latest project status.
Online simulation is not all: offline simulation can also be used: without access to the control system, configuration is simplified using a special offline variable editor, which can be used to set and display values.

Remote access via web
PASvisu uses the latest standardised Internet technologies such as HTML5, CSS3 and JavaScript.
JavaScript can be used to expand the functionality of the visualisation projects: pre-defined JavaScripts are available for calculations or scalings. As a result, users can shorten engineering time significantly and save costs.
As HTML5 is used, access is cross-platform and is possible via almost any end device such as PC, tablet or smartphone in the respective web browser. As an example, this facilitates remote maintenance that is based on genuine Client-Server functionality.
As a result, remote maintenance can be separated from on-site operation, helping to reduce downtimes.

Contact in the subsidiaries:

Don Gherashe
Telephone: +61 3 95446300

Great Britain:
Natasha Sephton-Pike
Telephone: +44 1536 460766

Shivani Handoo
Telephone: +91 20 24213994/95

Yvonne McNamara
Telephone: +353 21 4346535

USA and Canada:
Felicia Caponi
Telephone: +1 734 354-0211

Contact for the Pilz Group:

Martin Kurth
Corporate and Technical Press
Telephone: +49 711 3409-158

Sabine Karrer
Technical Press
Telephone: +49 711 3409-7009

Head office

Pilz Australia Safe Automation
Unit 1, 12-14 Miles Street
Mulgrave, Melbourne, Victoria 3170

Telephone: +61 3 9560 0621

Press contact

Telephone: 03 9560 0621