30 June 2016

PSENopt II in the final

The new type 3 light grids have reached the final of the GIT SECURITY AWARD 2017 in the "Safe Automation" category.

GIT SECURITY AWARD

A neutral jury with representatives from BHE, TÜV, VDMA, ZVEI and users nominated the finalists for the GIT SECURITY AWARD 2017. Three innovative products with the most votes were selected from five categories.  

Your vote counts! You can vote here for the PSENopt II; you have until 31 August 2016! All subscribers from Europe, Africa and the Middle East are eligible to vote.
 

The first type 3 light grids PSENopt II

The first type 3 light grids PSENopt II are designed for category PL d applications in accordance with IEC/EN 61496. They provide safety for finger and hand protection. Thanks to the absence of dead zones, PSENopt II can be installed with flexibility. With a shock resistance of 50 g, the light grids are extremely robust and so are ideally suitable for a rugged industrial environment.

Operators can use the LEDs to evaluate the causes of a machine stop plus any system defects. As a result, downtimes are minimised. In conjunction with control technology from Pilz, PSENopt II provide a a complete solution that's safe and economical for your plant. They can be connected directly to PDP67 using the 5-pin connector. Compatible assembly guides enable fast, simple installation.