Australia | english

17 Dec. 2014

What steps need to be considered when assessing and reducing risk?

Clear and compact - all the information is in our flowchart

The route from machine to safety function and its assessment in an appropriate assessment tool may be complex, but it is solvable. As a guide we have created the flowchart "Functional safety with EN ISO 12100, 13849-1 and EN/IEC 62061".
 

Risk reduction step-by-step

The flowchart describes at a glance the steps that need to be considered when assessing and reducing the risk from machinery. It also explains how safety functions can be evaluated and verified with EN ISO 12100, 13849-1 and EN/IEC 62061.

Download it now for free!

 

Further information: