Australia | english

1 Jan. 1970

PSS4000 - One system for all automation functions

With the all new PSS4000, Pilz brings a solution for all machine automation control and safety functions including motion control, diagnostics and visualization. The primary aim of the PSS 4000 is to simplify the decentralisation of control function s and reduce engineering work through the PAS4000 (Pilz Automation Suite) a groundbreaking new software platform which plays a key role in the system. It enables users to retain a centralised perspective of decentralised, distributed control structures. Because of its versatility the PSS4000 automation system can be used across a whole range of industries, for applications of any size.

 

With the all new PSS4000 automation system, Pilz has taken into account customers’ requirements for complete solutions, comprising safety and standard control technology. The PSS4000 is designed as an automation system for all industries: for mechanical engineering and the manufacturing sector alike. It’s a system that's easy to operate and considers the requirements for safety of man and machine from the outset.

PSS4000 enables you to reap the benefits of a decentralised control structure, without the increasing complexity normally involved. In terface problems associated with the connection of multiple control systems are a thing of the past.   As a result, when identical control programs and subfunctions are used decentralisation can help achieve a higher level of reusability and increase the level of standardisation. This in turn allows for a modular structure, so that identical components can be reused with minimum effort. The benefits can be seen in greater availability, due to local error reactions, and higher productivity as a result of shorter reaction times across the whole system.

 

A variety of programming languages available for selection

The PAS4000 software platform is used for all programming and parameter setting functions are fully compatible, with standard data and user interfaces. Not only does this make it easier to start working with or upgrade to PAS4000, it also means that multiple entries can be avoided, minimising the error sources which are often associated with manual data entry. PAS4000 offers established programming languages in accordance with IEC61131-3. What's more, Pilz has further developed the proven, easy-to-use configuration tool for the PNOZmulti safety system and, with PASmulti, provides its own editor, which is very user-friendly.

 

Components ease the burden of programming

Component-oriented programming is a key aspect of the PAS4000 software platform. Tested software blocks for common functions are available in a library, which can be expanded as necessary. An added new feature is the ability to expand this library with your own components.   The benefit can be seen in the high reusability of pre-defined functions and the reduced programming and engineering work.

Working with components means that programming can be separated from the hardware design, so that projects can be processed in parallel.

Once the machine functions have been standardised by creating components within libraries, it's quite simple to design the overall structure of the machine you wish to build, based on initial information. The detailed function can be determined later.

 

Symbolic addressing provides flexibility

With PAS4000 software platform, standard control functions and, for the first time safety functions too, can be completely created and managed symbolically. This mapping will be extended to the hardware at a later stage. All SafetyNET p devices will have direct access to this system-wide mapping table. The benefit being greater flexibility when implementing an application. This will have a positive impact not just during commissioning but also when changes are made later, because there will be no need to change the wiring. Neither will there be any problem exchanging hardware. Symbolic descriptions and addressing of periphery signals, programs and devices can be implemented across the board. Self-explanatory descriptions make it so much easier to find your way round the plant or machine when programming and during subsequent service functions.

 

Scalable hardware fits perfectly

The PSS4000 automation system is based on the proven, PSSuniversal decentralised I/O system. Head modules in various performance ratings have been developed in the PSS4000's first expansion phase; these are available for all safety-related and standard control functions. Connection to real-time Ethernet SafetyNET p is always a permanent component. SafetyNET p is used to network all the control components and transfers safety-related and non-safety-related data, as well as data for diagnostics, visualisation and motion control.

 

The PSS4000 automation system is an innovative alternative to system solutions.

When the PSS4000 was developed, the specific needs of safety technology were considered from the outset: The focus was on user-friendliness, high flexibility and universal support for the user during the whole engineering process.

With PSS4000, automation functions in the areas of safety and standard can be easily implemented across a whole range of industries – from small to medium-sized machinery, right through to large-scale plants.

F-PSS4000-unten-SL-378
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
Corporate and Technical Press

Telephone: +49 711 3409 - 158
E-Mail: m.kurth@pilz.de