Definitions and safety requirements in accordance with the Low Voltage Directive

Definitions and safety requirements in accordance with the Low Voltage Directive

Often there are other directives that need to be considered for plant and machinery, alongside the Machinery Directive. If a machine also contains electrical equipment, for example, then it will often fall under the scope of the Low Voltage Directive as well.

"For the purposes of this Directive, 'electrical equipment' means any equipment designed for use with a voltage rating of between 50 and 1 000 V for alternating current and between 75 and 1 500 V for direct current […]"

The Low Voltage Directive can be found on the homepage of the European Commission.

Official title of the Low Voltage Directive

DIRECTIVE 2014/35/EU OF THE EUROPEAN PARLIAMENT AND OF THE COUNCIL of 26 February 2014 on the harmonisation of the laws of the Member States relating to the making available on the market of electrical equipment designed for use within certain voltage limits

Related standards

EN 60947-1 to -8

Pilz Österreich

Pilz Ges.m.b.H. Sichere Automation
Modecenterstraße 14
1030 Wien
Österreich

Telephone: +43 1 7986263-0
E-Mail: pilz@pilz.at

Technischer Support

Telephone: +43 1 7986263-444
E-Mail: techsupport@pilz.at

Was this article helpful?