Is there a standard that states how high the reduced speed may be, on conveyors for example, if the conveyor is not enclosed?

Safe reduced speed and continuous flow conveyors

The C standard EN 619:2002 for continuous handling equipment and systems only states speed for cases in which people may travel on the conveyor. These are:

Continuous flow conveyors on which persons may travel:

  • Floor level: Conveying speed of 0.3 m/s
  • 0.3 m above floor level: Conveying speed of 0.15 m/s
  • Full railings: Conveying speed of 0.5 m/s

VDI 2854 also deals with the issue of safe, reduced speed. This states that a speed is deemed to be safe if the person has time to escape from a hazardous event.

 

Pilz Österreich

Pilz Ges.m.b.H. Sichere Automation
Modecenterstraße 14
1030 Wien
Österreich

Telephone: +43 1 7986263-0
E-Mail: pilz@pilz.at

Technischer Support

Telephone: +43 1 7986263-444
E-Mail: techsupport@pilz.at

Was this article helpful?