How can I read and save the error stack?

Software tool PNOZmulti Configurator

How can I read and save the error stack?

  1. Call up the error stack in the PNOZmulti Configurator; an online connection is needed.
  2. Using the right mouse button in the error text field, select all under the "Display" menu
  3. Then, under "Save", define the path and file name, ...
  4. ... save and email it to Technical Support (support@pilz.com).
    The file *.mperr can be displayed using any text editor (e.g. Windows text editor).

 

Pilz Österreich

Pilz Ges.m.b.H. Sichere Automation
Modecenterstraße 14
1030 Wien
Österreich

Telephone: +43 1 7986263-0
E-Mail: pilz@pilz.at

Technischer Support

Telephone: +43 1 7986263-444
E-Mail: techsupport@pilz.at

Was this article helpful?