- In the PNP configuration, the load is connected between the OSSD output and GND.
- With the NPN configuration, the load is connected between 24 VDC and the OSSD output switching element.
What is the difference between a PNP configuration and NPN configuration?
Safety light curtain PSENopt
Pilz Österreich
Pilz Ges.m.b.H. Sichere Automation
Modecenterstraße 14
1030 Wien
Österreich
Telephone: +43 1 7986263-0
E-Mail: pilz@pilz.at
Technischer Support
Telephone: +43 1 7986263-444
E-Mail: techsupport@pilz.at
Was this article helpful?