Austria | english

Sensor technology

Light beam devices PSENopt

What do we mean by the resolution of a light grid?

The device’s resolution is understood to be the minimum size that an opaque object must be to safely obscure at least one of the beams that form the scanning range.

The resolution is closely linked to the part of the body that requires protection.

  • Finger protection = 14mm
  • Hand protection = 30mm