Austria | english

Ostfildern, 23 Feb 2016

Pilz at the Hannover Messe 2016, Halle 9, Stand D17 - Your way of Automation!

Under the motto "We automate. Safely." Pilz will be presenting industry solutions and services for safety and automation at this year's Hannover Messe from 25 - 29.4.2016. The automation company will also be presenting its product innovations from the fields of "Sensor technology" – including a world first – and "Operating and monitoring".

Safe human-robot collaboration (HRC) will be another theme: visitors can be there live when our "robot colleague" swings into action. The company will be using a live demonstrator to illustrate how user-friendly the implementation of automation solutions for the Smart Factory can be, from engineering through to visualisation.

Premiere at HMI: Classy device!
A world first will be premiered on Pilz's stand: the new light grids PSENopt II are the first Type 3 light grid for use in applications in accordance with Category PL d of IEC/EN 61496. Since the standard changed in May 2015, users have had to switch to Type 4 if they wished to achieve PL d. In practice this leads to higher costs, when Type 4 is not even necessary. PSENopt II units bridge the gap in the standard and guarantee an economical light grid solution, because they are tailor-made.
The automation company will also be presenting another innovation in sensor technology with its new safety gate system PSENmlock. It offers safety gate monitoring with safe guard locking for personal and process protection up to the highest category PL e, all in one device.

Visualisation as a reliable observer
Pilz's sensor technology innovations include the new Safety Device Diagnostics, which comprise a fieldbus module, junction and safe sensor technology PSEN. Sensor diagnostics enable data to be called up simply, including at distance, thus reducing service operations and downtimes.
It's not only in sensor technology that a good overview ensures greater availability – Pilz can also provide support with a new complete solution for control, diagnostics and visualisation. In Hannover, the complete automation specialist will be presenting the new operator terminal PMI 6 Control from the PMI product series (Pilz Human Machine Interface), which is fitted with a soft PLC.

Robot colleague on the Pilz stand
As a complete supplier, Pilz offers services and solutions – such as the safe 3D camera system SafetyEYE – for safe robot applications.
In Hannover, our robot colleague will be handing over "a workpiece" to visitors – and not a disruptive guard in sight: a live demo on the Pilz stand will show how safe human-robot collaborations can already be realised today.
At the heart of the robotics presentation is the comprehensive services portfolio for this sector, which is tailored to the individual life phases of a robot system, providing support from process analysis and risk assessment to CE marking.

Just "Smart"
Alongside robotics, "Industrie 4.0" is another initiative on which the stand will focus. Here the company will use a live demonstrator to illustrate how control tasks in a modular plant can be efficient and user-friendly thanks to distributed intelligence. The focus in this case will be on the Industrie 4.0-compatible automation system PSS 4000.
As a member of the research platform SmartFactory KL, Pilz is actively involved in drafting uniform standards for Industrie 4.0. In Hannover, Pilz is also represented on the shared SmartFactory KL stand in Hall 8. On show will be a production line developed in conjunction with other partners, illustrating the practical application of some key aspects of Industrie 4.0.
 
"Big Partner" – USA is an important market for Pilz
Pilz has been represented locally with its own subsidiary in the USA for over 20 years. "This year's official partner country of the Hannover Messe is now the number one export market for German mechanical engineering and is an important market for Pilz", says Mike Beerman, General Manager of Pilz's American subsidiary. It provides support not only with solutions, but also with a comprehensive services portfolio: "Application knowledge about standards is important, because standards provide a framework for operators and users, enabling them to create a safe working environment. This is where Pilz USA can provide support", says Beerman.

Pilz is exhibiting at the Hannover Messe in Hall 9, Stand D17 and on the SmartFactory KL stand in Hall 8, Stand D20.

Further information at: www.pilz.com/de-DE/hannover-messe or under webcode web9481.


 

Under the motto
Under the motto

Under the motto "We automate. Safely." Pilz will be presenting industry solutions and safety and automation services at this year's Hannover Messe from 25 - 29.4.2016.

Headoffice

Pilz GmbH & Co. KG
Felix-Wankel-Straße 2
73760 Ostfildern
Germany

Telephone: +49 711 3409-0
E-Mail: pilz.gmbh@pilz.de

Pressekontakt

Telephone: +43 1 7986263-0
E-Mail: pilz@pilz.at