The various machine parts are linked earth-side to each other and to the general earthing terminal. Earthing generally occurs via a protective conductor incorporated into the machine's electrical connection cable.
With high power ratings the earth conductor may be positioned in the immediate vicinity of the supply cable, but it may not be incorporated within it.
These protective measures are met if the conductor cannot be replaced by the machine frame. They are not to be applied if the electrical work equipment has double insulation or reinforced insulation.