Not everyone’s a mathematical genius, which is why we developed the PAScal Safety Calculator. The software tool calculates and verifies the key safety parameters such as Performance Level (PL) and Safety Integrity Level (SIL) for plant and machinery safety functions. Our introductory film on PAScal shows you how easy it is to use the tool.
Safety assessment in compliance with current standards
With its systematic procedure, the PAScal Safety Calculator makes it easier for you to perform the safety assessment in compliance with current standards. The PAScal calculation is based on the harmonised safety standards EN ISO 13849-1 and EN/IEC 62061. The result is compared with the safety parameters required for the safety functions and is displayed in graphic form It is quite simple for you to see how individual components influence the respective safety functions.
For use across a range of manufacturers
The practical nature of the tool is impressive thanks to improved libraries, which store the safety-related characteristic data for all Pilz products and for other manufacturers from Sistema (Software Assistant produced by IFA). PAScal is simple and can be used quickly across a range of manufacturers.
Watch the introductory film on PAScal now.