With effect from 30.09.2011, the European Commission has published a new edition of the Official Journal for the EMC Directive. The Official Journal contains a current list of the standards harmonised under the EMC Directive 2004/108/EC and their reference data.
The new list is available under document number 2011/C288/01 and replaces the Official Journal 2011/C59/01, which previously applied. Following publication of the new EU Official Journal, the standards listed within the Journal can be regarded as harmonised under the EMC Directive 2004/108/EC. Only minor changes are involved, so most machine builders will not need to make any alterations.
Download
The document is available on the EU Document Server and via the following link.