Feeding material in safely without stopping production



Optoelectronic protective devices PSENopt provide maximum safety in panel production.
See the Industrial Automation magazine [Industrielle Automation] to discover which solution was implemented in practice.

Intelligent safety technology for pallet production machines

Roland Terwort GmbH & Co. KG manufactures machines as well as complete production lines for pallet production. The level of automation and complexity demands intelligent solutions on the part of the safety technology.

To achieve productivity while still safeguarding access to the work process, Terwort opted for optoelectronic protective devices PSENopt combined with the configurable control system PNOZmulti.

"Safety with perspective" with optoelectronic protective devices PSENopt

The safety light grid has a muting function, enabling material to be fed into the danger zone without stopping production, i.e. in areas in which the production process requires active intervention. The optoelectronic solution for area monitoring provides ergonomic, effective workplace protection, without obstructing the workflow. E-STOP pushbuttons and coded safety switches PSENcode also guarantee the safety of the block stacker in conjunction with the configurable control system PNOZmulti.

Read the full article here:
Link to Press Center

Further information:

Optoelectronic protective devices

Configurable safety relay PNOZmulti



Online Shopping here
Quicklinks
Webcode
Enter the 4-digit webcode:
Contact

Pilz Automation Safety L.P.
7150 Commerce Boulevard
Canton
Michigan 48187
Tel.: +1 734 354-0272
Fax: +1 734 354-3355
E-Mail: info@pilzusa.com

 

Follow us

Pilz RSS FeedYouTubeI Twitter 24I Facebook 24

 © Pilz GmbH & Co. KG 
8502