Would you like maximum safety for your plant, but shy away from a complex safety solution? Then you should get to know our new safety relay myPNOZ. We answer the most frequently asked questions about the new product.
Oct 12, 2021
The new safety relay myPNOZ
The new safety relay myPNOZ enables up to 8 independent safety zones to be monitored. These don't even need programming. You create them in no time using the online tool myPNOZ Creator. Want the machine to shut down quickly and reliably in an emergency? No problem: A global safety function is integrated into the head module of the myPNOZ. This affects all safety zones in an emergency and brings the machine safely to a stop. As a result, your staff and colleagues are always safe.
- The myPNOZ offers a global safety function via the head module as well as monitoring additional safety zones. What exactly does that mean?
The myPNOZ can monitor up to 8 different zones of a machine independently. As a result, individual areas of the machine can be stopped while others continue running. Also, the global safety function affects all zones of a machine – this enables the entire machine to be shut down, with an emergency stop for example.
- Which safety functions can be covered with the myPNOZ?
Safety functions such as emergency stop, safety gates, light curtains, Type IIIA/C two-hand pushbuttons and enabling switches can be monitored. #myPNOZ is suitable for small to medium-sized applications of low to medium complexity for monitoring from 2 to 16 safe input functions.
Pilz GmbH & Co. KG
Felix-Wankel-Straße 2
73760 Ostfildern
Germany
Telephone: +49 711 3409-0
E-Mail: pilz.gmbh@pilz.de
Americas
- Mexico: +52 55 5572 1300
- Brazil: + 55 11 4942-7032
- United States (toll-free): +1 877-PILZUSA (745-9872)
- Canada: +1 888-315-PILZ (315-7459)
Europe
- Ireland: +353 21 4804983
- Austria: +43 1 7986263-444
- Finland: +358 10 3224030 / +45 74436332
- Italy: +39 0362 1826711
- Russia: +7 495 6654993
- Spain: +34 938497433
- Denmark: +45 74436332
- Switzerland: +41 62 889 79 32
- Germany: +49 711 3409 444
- Belgium: +32 9 321 75 70
- Turkey: +90 216 5775552
- Netherlands: +31 347 320477
- France (toll-free): +33 3 88104000
- Sweden: +46 300 13990 / +45 74436332
- Portugal: +351 229 407 594
- United Kingdom: +44 1536 460866
Asia Pacific
- South Korea: +82 31 778 3390
- New Zealand: +64 9 6345350
- Japan: +81 45 471 2281
- Taiwan: +886 2 25700068
- Singapore: +65 6829 2920
- Thailand: +66 210 54613
- China: +86 400-088-3566
- Australia (toll-free): +61 3 9560 0621 / 1300 723 334