| DE FR ES IT NL
Finnish
Japanese
Polish
Portuguese
Chinese
Korean
Russian
Swedish
Turkish

Latest information - The very latest from Pilz

Latest Information    Press Archive   


Our press releases provide the latest news from the company and from the area of products and services.

The overview shows all the latest press releases at a glance.

Latest information
Ostfildern, January 18, 2012
Pilz and Thales Deutschland set the course – Safe, economical automation solutions for rail systems
Thales Deutschland and the automation company Pilz have concluded a co-operation agreement, with the aim of working together to develop products, functions and applications for signalling technology. Both partners are currently working on joint approval from the Federal Railway Authority (EBA) for an application with the highest safety requirement (CENELEC SIL4). The technical basis for these rail engineering solutions is the automation system PSS 4000 from Pilz.


Ostfildern, November 22, 2011
Pilz is visually underlining its development into a solution supplier for all automation tasks – The yellow band symbolises 4-fold safety
At the SPS/IPC/DRIVES 2011 exhibition in Nuremberg, Pilz is introducing its new brand presence to the public for the first time. With new advertising images and a new image the company is underlining its claim as a solution supplier for industrial automation.


Ostfildern, November 11, 2011
New generation of operator terminals PMI 509 and 515 with enhanced processors – Higher performance for diagnostics and visualisation
Higher performance and extended memory capacity thanks to enhanced 600 MHz RISC OMAP processors and high-contrast displays: These are the features of the new generation of Pilz operator terminals PMI (Pilz Machine Interface). The diagnostic units are now available in display sizes from 3.5" and with 5.7" screen diagonal. In conjunction with safe control technology from Pilz, they provide effective visualisation and troubleshooting support when production faults occur.


Ostfildern, October 26, 2011
Safe automation for a growth market – Pilz opens a subsidiary in India
Pilz GmbH & Co. KG has officially opened its subsidiary in India. Pilz India Pvt Ltd is based in Pune in western India and will provide product and service support to international customers as well as companies based or active in India. Plans to expand the subsidiary further are already underway. The commitment shown by Pilz shows its backing for greater safety awareness locally.


Ostfildern, October 12, 2011
Pilz at SPS/IPC/Drives 2011: Hall 9, Stand 9-370 – Safe one-stop automation
A holistic approach to automation is the focus of the Pilz stand at SPS/IPC/Drives 2011. Pilz offers a comprehensive portfolio of components, software and services for safety and standard. Key areas for Pilz at the exhibition for electrical automation will include Piilz's consultancy services en route to CE-marking, the Program Editor PASmulti and the "Safety and Automation Forum" featuring renowned experts on the stand in Hall 9, 9-370.


Ostfildern, September 30, 2011
The all-in-one motion control solution from Pilz – PMCprimo Drive P control system: Compact and powerful
With the control system PMCprimo DriveP Pilz is expanding its portfolio in the motion control sector. The new control system is a combination of motion control card and servo amplifier. PMCprimo DriveP is designed for applications with several axes and high requirements in terms of performance and synchronised movements. The compact dimensions, a fast processor, digital inputs and outputs, a clear software tool and the expandability with the PMCprotego S safety card are features of the new control system.



Pilz worldwide
Please select Your location

Pilz worldwide
Quicklinks
Webcode
Enter the 4-digit webcode:
 © Pilz GmbH & Co. KG 
0637