| DE FR ES IT NL

Safe 3D Vision - The Next Big Step in Safety

Melbourne, Jan 31, 2008

2008 will see the introduction of safe 3D vision with SafetyEYE from Pilz being released. But just what is safe vision and what are the advantages of using such a system?

Unlike conventional opto-electronic devices such as light curtains or laser scanners, a safe vision system can monitor multiple areas and detect foreign objects (such as a finger, leg etc.) within the viewing area, rather than detecting that a "light beam” has been interrupted.

There are two types of safe vision system that will be available – safe cameras (such as PSENvip) for press brake monitoring and safe 3D vision systems (such as SafetyEYE) for area monitoring.

A 3D safe vision system can monitor an area in 3 dimensions, compared with typical opto-electronic protection devices such as laser scanners or light curtain, which are 2-dimensional monitoring devices. This means with a 3D system you can specify height, width and depth, creating 3D monitoring zones anywhere in the viewing are, and the zones can be of any shape.

Current safety-related solutions have their limits

These limits are especially noticeable when you consider the example of a robot workstation comprising one or more robots and protected by safety fences.

To be able to detect people entering the danger zone or remaining within it, the robots generally require additional protective devices such as light grids and laser scanners in conjunction with a gate entry interlock.

However, typical optoelectronic protective devices are unable to monitor zones, at best they monitor planes. If there is no visual contact then the workstation must also be protected using pressure sensitive mats. So uninterrupted monitoring of a robot’s operating range is only possible with a great deal of technical investment, if at all. 
    

G-SafetyEYE-vorher-188

      
Figure 1 – Conventional sensors

   
Another factor is that standard protective devices immediately stop the robot in the case of danger. A restart costs time. With a safe vision system it can be different: In this case a detection zone violation does not automatically lead to an emergency stop. Warning functions may be triggered when a detection zone is violated, so that the robot continues at safely reduced speed. An emergency stop will only be triggered if the worker enters the immediate danger zone.

Last but not least, the large number of different components and the complex wiring involved makes it expensive to safeguard a robot workstation, and also has a negative impact on its availability.
    

G-SafetyEYE-nachher-560

        
Figure 2 – Safe 3D vision protection

   
Not only can a safe 3D vision system allow greater production productivity, but also maintenance tasks can be simplified. Cleaning the production area can be a lot easier without the requirement of removing or manoeuvring around fixed guarding, saving valuable time and money.

More information on the SafetyEYE safe vision system can be found at www.safetyeye.com.

To see an animated video of SafetyEYE please visit YouTube via this link: http://www.youtube.com/watch?v=YHEEeBerqUk
   

________________________________________________________________________________


Pass the word

If you have colleagues, associates, customers or suppliers who might like to receive this newsletter, please pass on the registration address http://www.pilz.com.au/newsletter.htm.


Suggestions?

Have a suggestion for a newsletter topic?
Please feel free to email any topic suggestions or feedback to us.


Unsubscribe

If you do NOT wish to receive any future issues please unsubscribe.

To manage your subscription, please go to our website.
  



Pilz worldwide
Please select Your location

Pilz worldwide
Shopping basket
0 Shopping basket items
Shopping basket
Quicklinks
Webcode
Enter the 4-digit webcode:
Careers with Pilz

Get detailed information here.

 © Pilz GmbH & Co. KG 
3966